AXIS#.ICONT

Description

AXIS#.ICONT returns the drive continuous rated current in Arms.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read Only

Units

Arms

Range

N/A

Default Value

N/A

Data Type

Float

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported.

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.ICONT

5000h

0bh

Signed32

-

1000:1

Read only

No

AXIS2.ICONT

5100h

0bh

Signed32

-

1000:1

Read only

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

5013

1

5013 (0x1395)

AXIS1.ICONT

Signed32

Read Only

Yes

70549

2

5013 (0x1395)

AXIS2.ICONT

Signed32

Read Only

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.ICONT

5013

Float

Read Only

-